This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: How many milliseconds the CC2 value of bq76952 is updated to MCU?

Part Number: BQ76952


Tool/software:

TI's experts,

    We plan to use MCU read the CC2 value of bq76952 through IIC communication. I would like to know how many milliseconds the CC2 value of bq76952 is updated to MCU?

    The project is quite urgent and we look forward to your response,

    Thank you.

  • Hi JMYang,

    The CC2 value is updated every ~3ms when FASTADC=0, every ~1.5ms when FASTADC=1, while the device is in NORMAL mode.  It is only updated at burst measurements while the device is in SLEEP mode, and isn't updated when in DEEPSLEEP or SHUTDOWN modes.

    Thanks,

    Terry