Tool/software:
Hi there,
sorry we tried to resolve the previous issue through a small board redesign but testing showed this issue wasn't solved at all.
What is supposed to happen
LM5171 is configured in DEM and shall boost 3.3 Vin and 5 Vin to the same 12 Vout, individually sinking up to 12 A at its input.
Problem:
Namely, CH2 only seems to not boost above a threshold under <1 A, last time it was 0.42 A, then 0.25 A, now under 0.5 A on the new PCB. CH2 was designed to be the exact copy of CH1, which happily boosts to 9+ A (didn't try higher but don't see why it could do it)
When varying ISET pin for CH2, the input current drawn first scales linearly as expected but quickly plateaus off. As in no matter what you set ISET voltage above, the current doesn't increase anymore at all and remains constant at this "plateau".
What we tried, and the result:
- 2x board redesigns, problem still persists
- half the Current sense resistor value by soldering another current resistor in parallel with the intention to plateau off at twice the current, plateau still appears at the same current as with one resistor.!
- flipping Channel 1 input and Channel 2 input with the intention to see if CH2 plateaus due to the low input voltage of 3.3 V. Instead, now CH1 can perfectly sink multiple Amps of 3.3 V and CH2 still has the same current plateau even with 5V from which it stops increasing in current.
In all cases, we have verified our Vin, Vout, ISET voltages and current measurements using multiple independent instruments.
What we haven't tried: Reading out LM5171 fault registers.
I have attached the schematics, .xlsx with the employed values, and a screenshot of the PCB. Do you see anything suspicious that could cause this plateau? Can't wait to send it off into production...
Thank you,
Karim
1057.LM5171 Buck or Boost Quickstart Tool_1.0.1.xlsxMA_tester_v1.pdf
Assembly drawing for a placement overview (LM5171 and SER1360-272 missing)
PCB design showing the layout more clearly, with orange (for FET gate drive) being Layer 3.