Tool/software:
Hi, I am new to the forum and am unable to get the LM27761 to work properly. R1 is 120K ohms, R2 is 100K ohms. I am using surface mount capacitors per the below schematic. They are all in the 0603 package and a combination of X7R and X5R low ESR, no greater than .03 ohms. Each component is on an adapter board which was professionally soldered on a hot air workstation. I have wired the circuit on a breadboard basically with very short or no leads at all. All 4 of the adapter thermal pads are tied to ground. I cannot get the output to be greater than -.35 volts. EN is tied directly to VIN. Any help would be appreciated.