Other Parts Discussed in Thread: BQ34Z100, EV2400, BQ41Z90, PMP23329
Tool/software:
Hi all,
We would like to protect a 9S LiPo battery pack and add a fuel gauge feature.
For protection, we are using the BQ7790522PWR with MOSFETs, everything is rated for 50A max. We’ve added a fuel gauge stage using the BQ34Z100-R2 to monitor the remaining capacity of the pack.
Could you please review the schematic and let us know if you notice any potential issues?
Our main concerns are:
-
Can we use the same shunt resistor for both ICs?
-
We plan to use the EV2400 to program the BQ34Z100, and then communicate over I2C with our C2000 microcontroller. Since the BQ7790522 cuts power on the low side, this means the microcontroller won’t share a ground with the BQ34Z100 during cutoff. We’ve added an I2C isolator — could you confirm whether we can power the isolator from REGIN, or should we generate a separate 5V_ISO rail?
-
If you are aware of a single IC that combines both protection and fuel gauge functionality for 9S LiPo packs, we’d love to hear about it.
- If the circuit remains connected while the battery is in storage, could it cause unwanted current draw and slowly drain the pack? Should we add a switch or another method to fully disconnect it?
Thank you,
BatteryProtector_FuelGauge.pdf