Other Parts Discussed in Thread: LMG1210
Tool/software:
As mentioned in the above forum, how can i use the second methodology mentioned?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
LMG1020 can be used as a high side driver using an isolated floating supply as shown in the diagram. The driver ground pin, IN- pin, and floating supply negative is connected to the switch node/high side FET source. The floating supply positive is connected to VDD. A level shifter may be needed in the IN+ input to translate the ground referenced signal to the floating supply referenced input.
If you need to drive a GaN half bridge configuration, our LMG1210 device includes a low side driver and high side driver with level shifter.
Thank you,
Walter