This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54260-Q1: Minimum inductor ripple current required

Part Number: TPS54260-Q1

Tool/software:

Hello,

In the datasheet it is mentioned minimum inductor to be 150mA.

In my application the minimum current itself is 140mA. If i consider kind factor of more than 1.0 then ripple current increase but inductor current will go negative/ discharge fully.

Is it a hard rule to consider minimum ripple current of 150mA?

Thank you,