Tool/software:
Hello,
we have a product that needs OTP programming, and I created a software for a programming tool according to the sequence at 3.1 in SLUAA32A.
We noticed that when there is an hardware problem, where the diode equivalent of the D1 in your dev board BQ76952EVM (that feeds power to BAT and CP1 pins) is not soldered properly, at the end of the OTP sequence the BM reports a successful OTP but if I power cycle the device, it is still blank. This refers to the step "...Read from 0x40 to check if OTP programming was successful (0x80 indicates success)."
Is there a way to read directly the OTP memory, instead of just reading the RAM? I can not reset the IC to verify the OTP sequence because I have enabled the permanent failure, so at the next reset, with a voltage < 12V, it would flash a permanent fail for cell undervoltage.
Thanks