Part Number: LM5176
Tool/software:
I'm Having problems with the following design:
I'm new at with this product. I used the WEBENCH Power Designer for 12V-30V in and 12V 11A out.
It works fine for 12V power supply I get 12Vout and 4A. However, when I power it with a 24V-28V power supply, I get 5V out. Going back to the 12V power supply I still get 5V out.
The only this I haven't done was "John Wallace 1" suggestion to use 0hm resistors for each gate driver.
I manufactured 10 boards and have lost 6 of them and using them to blink LEDs at 80ms on/off.
I'm using the following MOFSETS: CSD17577Q5AT, CSD17577Q5AT, CSD18514Q5AT, and CSD18534Q5AT.

Is there something I'm missing?
Will the 0hm resistors help?