This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB-TO-GPIO2: My test PC with Windows server 2008 R2 cannot recognize USB2GPIO v2.0.

Part Number: USB-TO-GPIO2


Tool/software:

I need to use USB2GPIO  Interface Adapter Evaluation Module to do power sequencing for my PCBA. My computer OS is Windows server 2008 R2.

When I plug-in USB2GPIO  to USB port,  Device Manager shows unknown device, Device status shows the drivers for this device is not installed.

When I tried to update driver software  and searched it in Internet, I could not find the driver software. 

Can TI  help to get USB2GPIO driver software which is compatible to Windows server 2008 OS ?

  • Hello, 

    There are no such drivers for USB-TO-GPIO2. The adapter is designed to be plug-and-play with no need for driver installation. I recommend trying the adapter on a different pc

    Adapter Module User Guide:

    Best regards,
    Britton