This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSF12C1: Active EMI Filter Evaluation Module for Single-Phase AC Power Systems

Part Number: TPSF12C1

Tool/software:

we are working on EMC passive standard filter for power board (3.7KW max). 

power board is connected to main line 230VAC @ 50Hz (MAX input current 15A rms) and use several half-bridge inverter that works with switching frequency of 70KHz.

with standard passive filter we are not able to respect the standard EN55014 for conducted emission.

I need information if is possible to use AEF solution for our power level (3.7KW)?

i studied the datasheet of evaluation board TPSF12C1QEVM where the application's power is not mentioned so i need to understand if this solution could be integrated on my project.

second our big problem is the space on the filter board and with traditional passive common mode choke that are bigger.

is possible to have a support from  FAE in order to discuss about our problem.

attach a report where we explain our filter solutiona frequency spectrum of conducted emission.

report EMC condotte eng.pdf