Other Parts Discussed in Thread: BQ25756
Tool/software:
Building a 240W source and wondering if there are any "plug and play" buck converters that can be used, or do I need a MCU, DAC and buck converter?
What I want is to build a source with full PPS/AVS capability. Input will likely be 48V/5A, TPS26750 as PD controller, then I will need to switch the output voltage to what the sink request, so I2C->DAC/switch regulator
I have not seen any chip that does this, only charging.
I understand I can use the GPIOs to trigger fixed voltages, but can I do it easily for PPS/AVS, or do I need an MCU as a translator?