Tool/software:
Hi TI:
I simply used BQ25672 to charge the battery(2S 18650), And all the configurations use the default settings. When I plugged in the battery to start charging, the following situation occurred:
[ Input Vol: 9.0V ]
Q1. The battery can be charged normally, but the current is relatively low (about 0.7A, the default config is 1A);
Q2. Sometimes, when inserting the battery, the charging current is only 0.25A to 0.45A , And the BQ25672 and Inductance shows obvious signs of overheating (about 40~50℃). And now the SW1/2 is 4.2V;
[ Input Vol: from 6V to 9V (Use a variable power supply) ]
Q3. When the input voltage gradually increased from 6V to 9V, the battery failed to charge properly.
This is my schematic:
This is my layout (Two-Layer):
Register dump for the above three problem points:
Dump registers in Q1:
0x12 0x03 0x48 0x00 0x64 0x4c 0x00 0x9c 0xc3 0x05 0x63 0x00 0xdc 0x4b 0x3d 0xa2 0x85 0x40 0x00 0x21 0x1e 0xaa 0xc0 0x7a 0x54 0x00 0x9c 0x2f 0x8a 0x01 0x00 0x00 0x00 0x00 0xaf 0x92 0x50 0x1c 0x20 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x30 0x00 0x00 0x00 0x00 0x00 0x00 0x23 0x67 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x21
Dump registers in Q2 (Charge current is 0.42A with overheating):
0x12 0x03 0x48 0x00 0x64 0x4c 0x00 0x98 0xc3 0x05 0x63 0x00 0xdc 0x4b 0x3d 0xa2 0x85 0x40 0x00 0x21 0x1e 0xaa 0xc0 0x7a 0x54 0x00 0x98 0x2f 0x6a 0x01 0x00 0x00 0x00 0x01 0xaf 0x92 0x50 0x18 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x30 0x00 0x00 0x00 0x00 0x00 0x00 0x23 0x61 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x21
Dump registers in Q3:
0x12 0x03 0x48 0x00 0x64 0x26 0x00 0x98 0xc3 0x05 0x63 0x00 0xdc 0x4b 0x3d 0xa6 0x85 0x40 0x00 0x21 0x1e 0xaa 0xc0 0x7a 0x54 0x00 0x32 0x27 0x0a 0x01 0x00 0x00 0x00 0x00 0xdf 0x92 0x50 0x18 0x20 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x30 0x00 0x00 0x00 0x00 0x00 0x00 0x11 0xaa 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x21