Other Parts Discussed in Thread: EV2400
Tool/software:
Good morning,
We designed a 4S battery for our controllers using the BQ76952. I'm attaching the config file set by the EV2400.
We are not interested in the SLEEP mode, and have set the SLEEP (Bit 8) in the Power Config Register to be 0. However, we are noticing the 4S battery would go into SLEEP mode when it's completely discharged. It doesn't allow for charging.
We want our users to be able to charge the battery once it's goes dead.
I'm also attaching the config file after it goes into SLEEP mode and automatically changes the SLEEP (Bit 8) in the Power Config to 1. How can we avoid this situation? It's holding us from shipping our unit out.
BQ76952_4S_8A_NoSleep_R1.gg.csv
The config file below was exported after it goes into SLEEP mode (when completely discharged).