This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2981-N: Restricted Chemicals Certificated and REACH and RoHS - LP2981AIM5-5.0/NOPB

Part Number: LP2981-N


Tool/software:

Hi, 

I would like your support in answering the following questions relating to part number:  LP2981AIM5-5.0/NOPB

These queries are part of our companies internal part qualification for the Medical Device Market. 

Q 1  Presence of substances listed in REACH   Annex XIV as amended or CLP  Annex VI Part 3 as carcinogenic, mutagenic or toxic to reproduction of category 1A or category 1B ( ≥ 0.1% by weight)

Q 2   Presence of substances having endocrine disrupting properties according to Article 59 of REACH1 as amended ( ≥ 0.1% by weight)

Q 3   Presence of substances listed in REACH1 Annex XVII or candidate list ( ≥ 0.1% by weight)

Q 4   Presence of RoHS 3 restricted substances ?

Q 5   Have you completed any SCIP  notifications?

Q 6   Presence of PROP65  substances above the Safe Harbor Level?

Q 7   Presence of substances with animal origin

Q 8   Presence of Latex or natural rubber

Q 9   Safety Data Sheets (SDS) and Test Data included confirming compliance to the information listed above

Q 10  What is the status of the environment where you manufacture this component (General manufacturing, controlled environment, clean room)?
Id expect the component meets these requirements however we need to provide evidence that it does in fact do that. 
Kind regards
Noel