Tool/software:
Dear Support,
I work on the EVM65987DDK with a 10G-Expansion-EVM attached to a 1GB USB3 to LAN Bridge.
GPIO7 is used to switch between two virtual devices to get different output power stages.
Without activating the GPIO Event the USB Device is recogniced an working well, after activating the GPIO Event the USB Device still working on a Android Tablet but not on Windows10/11.
Do I have a problem with recourses on the TPS65987DDK or have I to set some aditional settings.
Has anyone a idea what I can do to get this working on both devices
attached you can find my project-file
Test_2 Thinkpad Samsung HP GPIO_7.pjt
Thank you verry much
Martin Jäger