Tool/software:
Hello guys,
One of my customers is considering using TPS56638.
They are checking TPS56638 performance using Webench.
At this moment, they have the following questions.
Could you please give me your reply?
Q1.
They run TPS56638 Webench with Vin=12V(Min, Max), Vout=3.3V, Iout=6A.
Also they set "Minimum Inductor Current Rating" in Configuration Options to "Peak Current".
As the result, SPM6530T-1R5M100 (1.5uH, IDC=10A) inductor was chosen for L1.
At next, they changed "Minimum Inductor Current Rating" in Configuration Options to "Current Limit" and clicked "REDESIGN".
As the result, XAL7070-182MEB (1.8uH, IDC=21A) inductor was chosen for L1.
What is difference between "Peak Current" and "Current Limit" of "Minimum Inductor Current Rating"?
And how to use "Minimum Inductor Current Rating" setting?
Q2.
IDC of XAL7070-182MEB chosen by Webench in "Current Limit" case was 21A.
The customer think this IDC value is too large compared with L1 peak current (about 7.2A).
Why did Webench chose the inductor which has such large IDC?
Your reply would be much appreciated.
Best regards,
Kazuya.