Other Parts Discussed in Thread: EV2400
Tool/software:
Hello team,
I'm using BQ34210 EVM for fuel gauge with EV2400 module.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello team,
I'm using BQ34210 EVM for fuel gauge with EV2400 module.
Hello,
Please refer to section 1.3.3.8 from the BQ34210 Technical Reference Manual.
Regards,
Jonny.
Hi,
Today's observation - I have tried to do learning cycle of battery in which charging of the battery has been finished then it went to relax mode later when i'm trying to do discharge of the battery for that i have enabled EOS_START_LEARN then LFAULT and LDPAI flag has been arisen.
kindly check the log file which is been attached here.
Regards,
Subhiksha
Fri Jul 18 19:46:11 IST 2025 Device Name = bq34210 Firmware Version = 0_03 Design Capacity = 10000 Sample,DateTime,ElapsedTime,Control,Voltage,Batt Stat,Current,Temperature,RSOC,RemCap,FullChgCap,AvgCurr,AvgPwr,RunTimeEmty,AvgTimeFull,AccumulatedCharge,AccumulatedCharge Time,IntTemp,CycleCnt,SOH,ChgVolt,ChgCurr,BLTDsgSet,BLTChgSet,OpStat,GaugeStat,EDV Threshold,CEDVRemCap,SmRemCap,SmCurrent,ManufacStat,EOSLearnStatus,EOSSafetyStatus,EOSStatus,AutoLearnTime,AvgDsgCurrent,AvgDsgTemp,LearnedResistance,LearnedResTimeHours,LearnedResTimeSeconds,LastLearnedResistance,LastLearnedResHours,LastLearnedResSeconds,InitialRRateAgeHours,InitialRRateAgeSeconds,RRate,RRateLong,InitialRcellRRateLearnRes,InitialRcellRRateLearnCount,LogRowTime(ms),LogStatus 1,2025-07-18 19:46:15,4.011,0x0000,3945,0x0000,-30,25.8,82,1797,2200,-30,-12,3594,65535,54,29,25.8,0,22,4200,1100,150,175,0x0802,0x140,3648,1797,1797,0,0x05,0x1141,0x00,0x10,2857,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,617,SUCCESS 2,2025-07-18 19:46:19,8.013,0x0000,3945,0x0000,-30,25.8,82,1797,2200,-30,-12,3594,65535,55,29,25.8,0,22,4200,1100,150,175,0x0802,0x140,3648,1797,1797,0,0x0D,0x0000,0x00,0x10,5399999,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,597,SUCCESS 3,2025-07-18 19:46:23,12.014,0x0000,3945,0x0000,-30,25.8,82,1797,2200,-30,-12,3594,65535,55,29,25.8,0,22,4200,1100,150,175,0x0802,0x140,3648,1797,1797,0,0x0D,0x0000,0x00,0x10,5399995,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,611,SUCCESS 4,2025-07-18 19:46:27,16.028,0x0000,3945,0x0000,-30,25.8,82,1797,2200,-30,-12,3594,65535,55,29,25.8,0,22,4200,1100,150,175,0x0802,0x140,3648,1797,1797,0,0x0D,0x1011,0x00,0x10,5399991,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,601,SUCCESS 5,2025-07-18 19:46:31,20.036,0x0000,3945,0x0000,-30,25.8,82,1797,2200,-30,-12,3594,65535,55,29,25.8,0,22,4200,1100,150,175,0x0802,0x140,3648,1797,1797,0,0x0D,0x1141,0x00,0x10,3598,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,611,SUCCESS 6,2025-07-18 19:46:35,24.043,0x0000,3945,0x0000,-30,25.8,82,1797,2200,-30,-12,3594,65535,55,29,25.8,0,22,4200,1100,150,175,0x0802,0x140,3648,1797,1797,0,0x0D,0x1141,0x00,0x10,3594,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,599,SUCCESS 7,2025-07-18 19:46:39,28.054,0x0000,3945,0x0000,-30,25.8,82,1797,2200,-30,-12,3594,65535,55,29,25.8,0,22,4200,1100,150,175,0x0802,0x140,3648,1797,1797,0,0x0D,0x1141,0x00,0x10,3590,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,620,SUCCESS
Hello,
Please see the following from the TRM. It explains the behavior you are seeing.
Regards,
Jonny.
Hi Team,
Thanks for your reference.
For discharging battery, we have given 30mA of current still it is going to LFAULT only.
Can you tell me how much current should i give for discharging of battery and how long will it take for complete discharge?
And after discharging how long will it be in relaxation mode?
Regards,
Subhiksha
Hi,
Sorry for this, the E2E thread which you mentioned didn't resolve my issue.
LFAULT and LDPAI flag is keep on coming if I'm trying to charge and discharge of the battery as well.
if possible, can you arrange respective person to connect through call asap to resolve this issue.
Regards,
Subhiksha.
Hello,
Please ensure you have an accurate temperature reading. Typically these flags are set when the temperature is too high or too low. Additionally please ensure you have completed the temp calibration.
Regards,
Jonny.
Hello,
I have successfully completed the temperature calibration, then I have tried learning cycle- (charging the battery) still I'm getting the same error.
here I have attached the observation logs.
kindly check and guide me what to do.
Regards,
Subhiksha
Tue Jul 29 15:51:39 IST 2025 Device Name = bq34210 Firmware Version = 0_03 Design Capacity = 10000 Sample,DateTime,ElapsedTime,Control,Voltage,Batt Stat,Current,Temperature,RSOC,RemCap,FullChgCap,AvgCurr,AvgPwr,RunTimeEmty,AvgTimeFull,AccumulatedCharge,AccumulatedCharge Time,IntTemp,CycleCnt,SOH,ChgVolt,ChgCurr,BLTDsgSet,BLTChgSet,OpStat,GaugeStat,EDV Threshold,CEDVRemCap,SmRemCap,SmCurrent,ManufacStat,EOSLearnStatus,EOSSafetyStatus,EOSStatus,AutoLearnTime,AvgDsgCurrent,AvgDsgTemp,LearnedResistance,LearnedResTimeHours,LearnedResTimeSeconds,LastLearnedResistance,LastLearnedResHours,LastLearnedResSeconds,InitialRRateAgeHours,InitialRRateAgeSeconds,RRate,RRateLong,InitialRcellRRateLearnRes,InitialRcellRRateLearnCount,LogRowTime(ms),LogStatus 1,2025-07-29 15:51:43,4.009,0x0000,3951,0x0002,170,24.4,69,1512,2200,170,67,65535,243,-154,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1512,1512,0,0x0F,0x0000,0x00,0x10,5396731,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,608,SUCCESS 2,2025-07-29 15:51:47,8.020,0x0000,3951,0x0002,170,24.4,69,1512,2200,170,67,65535,243,-154,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1512,1512,0,0x0F,0x0000,0x00,0x10,5396727,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,612,SUCCESS 3,2025-07-29 15:51:51,12.026,0x0000,3951,0x0002,170,24.4,69,1513,2200,170,67,65535,242,-155,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1513,1512,0,0x0F,0x0000,0x00,0x10,5396723,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,607,SUCCESS 4,2025-07-29 15:51:55,16.038,0x0000,3950,0x0002,170,24.4,69,1513,2200,170,67,65535,242,-155,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1513,1512,0,0x07,0x0000,0x00,0x10,5396720,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,610,SUCCESS 5,2025-07-29 15:51:59,20.050,0x0000,3951,0x0002,170,24.4,69,1513,2200,170,67,65535,242,-155,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1513,1513,0,0x0F,0x0000,0x00,0x10,5399999,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,601,SUCCESS 6,2025-07-29 15:52:03,24.064,0x0000,3951,0x0002,170,24.4,69,1513,2200,170,67,65535,242,-155,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1513,1513,0,0x0F,0x0000,0x00,0x10,5399995,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,601,SUCCESS 7,2025-07-29 15:52:07,28.070,0x0000,3951,0x0002,170,24.4,69,1513,2200,170,67,65535,242,-155,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1513,1513,0,0x0F,0x0000,0x00,0x10,5399991,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,608,SUCCESS 8,2025-07-29 15:52:11,32.075,0x0000,3951,0x0002,170,24.4,69,1514,2200,170,67,65535,242,-156,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1514,1513,0,0x0F,0x0000,0x00,0x10,5399987,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,605,SUCCESS 9,2025-07-29 15:52:15,36.086,0x0000,3951,0x0002,170,24.4,69,1514,2200,170,67,65535,242,-156,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1514,1513,0,0x0F,0x0000,0x00,0x10,5399983,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,611,SUCCESS 10,2025-07-29 15:52:19,40.094,0x0000,3951,0x0002,170,24.4,69,1514,2200,170,67,65535,242,-156,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1514,1513,0,0x0F,0x0000,0x00,0x10,5399979,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,602,SUCCESS 11,2025-07-29 15:52:23,44.095,0x0000,3951,0x0002,170,24.4,69,1514,2200,170,67,65535,242,-156,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1514,1514,0,0x0F,0x0000,0x00,0x10,5399975,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,600,SUCCESS 12,2025-07-29 15:52:27,48.110,0x0000,3951,0x0002,170,24.4,69,1514,2200,170,67,65535,242,-156,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1514,1514,0,0x0E,0x0000,0x00,0x10,5399971,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,617,SUCCESS 13,2025-07-29 15:52:31,52.116,0x0000,3951,0x0002,170,24.4,69,1515,2200,170,67,65535,242,-157,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1515,1514,0,0x0E,0x0000,0x00,0x10,5399967,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,613,SUCCESS 14,2025-07-29 15:52:35,56.124,0x0000,3951,0x0002,170,24.4,69,1515,2200,170,67,65535,242,-157,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1515,1514,0,0x0E,0x0840,0x00,0x10,3599,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,602,SUCCESS 15,2025-07-29 15:52:39,60.126,0x0000,3950,0x0002,169,24.4,69,1515,2200,169,67,65535,243,-157,11,24.4,0,22,4200,1100,150,175,0x0882,0x00,0,1515,1514,0,0x0E,0x0840,0x00,0x10,3595,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,599,SUCCESS
Hi Jonny,
Sure, I have shared a log file with this.
Moreover, can you tell me why we are getting LFAULT and LUCD flag. What could be the solution?
I'm waiting for your reply.
Regards,
Subhiksha
Hi Jonny,
FCC is not yet estimated even after completion on charging the battery.
so, can you tell me when it will be estimating the FCC value what is the procedure to be followed to find FCC value.
whether we have to complete charging as well as discharging cycle also to estimate the FCC value?
please check the previously sent logs which has been observed during charging and discharging the battery .
and let me know how to resolve the LFAULT flag.
Regards,
Subhiksha
Hi Jonny,
Today's log observation has been attached here.
Kindly help me to resolve those errors.
I need a solution for previous query also.
Thu Aug 07 15:04:56 IST 2025 Device Name = bq34210 Firmware Version = 0_03 Design Capacity = 1000 Sample,DateTime,ElapsedTime,Control,Voltage,Batt Stat,Current,Temperature,RSOC,RemCap,FullChgCap,AvgCurr,AvgPwr,RunTimeEmty,AvgTimeFull,AccumulatedCharge,AccumulatedCharge Time,IntTemp,CycleCnt,SOH,ChgVolt,ChgCurr,BLTDsgSet,BLTChgSet,OpStat,GaugeStat,EDV Threshold,CEDVRemCap,SmRemCap,SmCurrent,ManufacStat,EOSLearnStatus,EOSSafetyStatus,EOSStatus,AutoLearnTime,AvgDsgCurrent,AvgDsgTemp,LearnedResistance,LearnedResTimeHours,LearnedResTimeSeconds,LastLearnedResistance,LastLearnedResHours,LastLearnedResSeconds,InitialRRateAgeHours,InitialRRateAgeSeconds,RRate,RRateLong,InitialRcellRRateLearnRes,InitialRcellRRateLearnCount,LogRowTime(ms),LogStatus 1,2025-08-07 15:05:00,4.008,0x0000,4053,0x0098,-5,24.7,100,2185,2200,-5,-2,26220,65535,13,37,24.7,0,100,4200,0,150,175,0x0882,0x14A,0,2185,2185,0,0x0F,0x0000,0x00,0x10,5399999,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,618,SUCCESS 2,2025-08-07 15:05:04,8.015,0x0000,4053,0x0098,-5,24.7,100,2185,2200,-5,-2,26220,65535,13,37,24.7,0,100,4200,0,150,175,0x0882,0x14A,0,2185,2185,0,0x0F,0x0000,0x00,0x10,5399995,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,608,SUCCESS 3,2025-08-07 15:05:08,12.024,0x0000,4053,0x0098,-5,24.7,100,2185,2200,-5,-2,26220,65535,13,37,24.7,0,100,4200,0,150,175,0x0882,0x14A,0,2185,2185,0,0x0F,0x0000,0x00,0x10,5399991,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,621,SUCCESS 4,2025-08-07 15:05:12,16.027,0x0000,4053,0x0098,-5,24.7,100,2185,2200,-5,-2,26220,65535,13,37,24.7,0,100,4200,0,150,175,0x0882,0x14A,0,2185,2185,0,0x0F,0x0010,0x00,0x10,5399987,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,614,SUCCESS 5,2025-08-07 15:05:16,20.030,0x0000,4053,0x0018,-5,24.7,100,2185,2200,-5,-2,26220,65535,13,37,24.7,0,100,4200,0,150,175,0x0882,0x14A,0,2185,2185,0,0x0F,0x1011,0x00,0x10,5399983,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,614,SUCCESS 6,2025-08-07 15:05:20,24.044,0x0000,4053,0x0098,-5,24.7,100,2185,2200,-4,-2,32775,65535,13,37,24.7,0,100,4200,0,150,175,0x0882,0x14A,0,2185,2185,0,0x0F,0x1141,0x00,0x10,3599,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,628,SUCCESS 7,2025-08-07 15:05:24,28.052,0x0000,4053,0x0098,-5,24.7,100,2185,2200,-4,-2,32775,65535,13,37,24.7,0,100,4200,0,150,175,0x0882,0x14A,0,2185,2185,0,0x0F,0x1141,0x00,0x10,3595,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,606,SUCCESS
Regards,
Subhiksha.
Hello,
This log file still does not show the entire learning cycle. This only shows 7 data points which is not the entire charge and discharge. Please attach the full log file.
Regards,
Jonny.