Part Number: BQ76952
Tool/software:
Hi TI team,
I’m working with the BQ76952 in a 16S Li-ion battery application. I’m trying to enter Shutdown mode by pulling the RST_SHUT pin high for more than 1 second, but the device does not seem to shut down.
Here are the details:
- REG1 is active and supplying 2.2V
- RST_SHUT pin is pulled high to 3.3V for >1s
- No I2C/SPI communication during this time
- FETs are off, no PF or Alarm active
Is there any other condition that could be preventing Shutdown mode? Any suggestion is appreciated.
Best regards,
Vic