This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR51635: Switching pin ringing noise

Part Number: LMR51635


Tool/software:

Dear technical support:

I'm using LMR51635YDDR, 1.1MHz switching frequency (because I use two DC/DC converter parallel, besides LMR51635, another is LMR22676, 500KHz, from one paper it said when DC/DC converters are parallel, the switching frequency shall be different, so I use 1.1MHz version). the board input 24Vdc, output 5VDC/3A, everything works fine, but it fails EMC radiated emission test, I test pin 5-SW, it has 50MHz ringing noise, I try to add RC snubber circuit to decrease it, it doesn't work, when cap increase to 1300pf/8R ohm, it works, when using 220pFcaps, the output voltage is unstable, from datasheet the SW pin 5, it is push-pull output, could you please tell me how to decrease the ringing noise in pin 5? thank you very much!

Regards

Julia Zhou