Tool/software:
We have developed a power module using the TPS65400 PMIC to power the XC7Z020 Zynq SoC. The module includes a provision for a 5x2 header compatible with USB-to-Any interface for configuration and monitoring via the Fusion Digital Power Designer tool.
All four power rails (SW1 to SW4) have been configured with the following voltage and timing parameters:
-
SW1 – 1.0 V, TON/TOFF Delay: 5 ms
-
SW2 – 3.3 V, TON/TOFF Delay: 0 ms
-
SW3 – 1.8 V, TON/TOFF Delay: 25 ms
-
SW4 – 1.35 V, TON/TOFF Delay: 100 ms
During testing, we confirmed that all voltage rails are physically ON at their respective outputs, verified using a multimeter.
However, the GUI dashboard does not display any Output Voltage (OV) readings — it shows either zero or blank values for all channels. This persists even though the rail voltages are present on the board.
We have attached the configuration file (*.tifsp
) for your review.
Kindly advise if any additional registers or telemetry settings need to be enabled to allow proper OV monitoring on the GUI.