Part Number: TPS5430
Tool/software:
I'm using the TPS5430DDAR in my circuit. The input voltage is 24V nominal, with a maximum of 30V, and the output is 5V at 200mA. However, the IC is heating up to 55 to 60°C.
So far, the output voltage and current are stable and accurate there’s no visible issue with performance. But I’m concerned about the heat during long-term operation, especially since we plan to use this part in mass production.
-
Could there be any issue with my design causing this heat?
-
Will this temperature affect long-term reliability?
-
What suggestions do you have to reduce the heat dissipation?