This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25037: Push-Pull controller

Part Number: LM25037
Other Parts Discussed in Thread: , UCC2808A-2

Tool/software:

Hello Team,

I am looking for and DCDC controller for following application:

  • Input voltage: From Battery ~7V
  • Output voltage: Configurable to 250V and 420V
  • Output Current: Max 800mA @ 500usec PRF (Load: Capacitor with 500Ohm)

I was suggested Push-Pull controller from Texas on e2e forum ( LM5185-Q1: DCDC for 7V (input) to 32V (Output) )

AC/DC & DC/DC controllers (external FET) product selection | TI.com

UCC2808A-2Q1 data sheet, product information and support | TI.com

I am looking forward for UCC2808A or LM25037-Q1 as both have similar input range but LM25037 has additional features.

1. Could you please share some TI guide for component selection like MOSFET/ Transformer for Non-Isolated design?

2. Parts UCC2808A and LM25037-Q1 are not listed on TI webench and PowerDesigner web tool for above application.

Regards