This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2121: I think the output current is not up to 4.5A,what can i do that can improve the output current?

Part Number: TPS2121


Tool/software:

0488.pdf

I want to design a circute that can  output 4A current,like show in the pdf.but the actually out is  about  2A,how can i improve it?