This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8868X-Q1: Inquiry Regarding LP8868-X Boost Topology for 46W LED Load

Part Number: LP8868X-Q1

Tool/software:

Dear Sir,

I hope you're doing well.

I would like to confirm whether the LP8868-X, configured in boost topology, is capable of handling a load of 46 watts consisting of 12 LEDs, each with a forward voltage of 3.2V. I have attached the document here.

Based on the datasheet, I understand that the LP8868-X supports boost operation with an input voltage range of 4.5V to 65V and can deliver up to 4A output current. However, I would appreciate your guidance on whether this configuration is suitable for the specified LED setup, especially in terms of power handling.

Looking forward to your expert advice.

Best regards,

Rabina

LP8868.docx