Tool/software:
Hello,
I’m working with a 4-cell LiFePO4 battery pack (12.8 V nominal, 3.6 Ah). I’ve noticed about 10% capacity loss within 4 weeks on some packs. After a quick check, I found that the logs show Cell 2 and Cell 4 reaching 3.8 V, while the others remain lower.
The packs are charged at 14.4 V, 750 mA. I ran a full charge cycle and logged the cell voltages on the graph, Cells 2 and 4 consistently rise higher than Cells 1 and 3, especially toward the end of the charge.
When the batteries are left to rest, the voltages eventually balance out, but the imbalance is clear during charging.
Does anyone know why such a large difference appears between the cells during charge and is there anything I can do to help?
Kind Regards,
Mike