Tool/software:
I use LMG3410-HB-EVM as the high freq. arm of my totem-pole PFC. It was broken three weeks ago, and I have fixed it many times, the heat of the Upper arm switch still higher then expected, especially when I supply 5V for this board, and the problem gets worse and worse. The FAULT of Upper arm is low level yesterday when i fixed it last time, before then, it is high level and I didn't detect any obvious short or signal abnormality. I think whether I broken a layer of board when I re-solder the switches.I use full bridge rectification to test whether the circuit is corrected, if i don't supply 5V for this board, the positive half cycle of input current is higher then negative one for about 0.1mA. Otherwise, there're only positive half cycle of input current. By the way, the specification of the circuit is: 230Vrms for Input Voltage; 400V for Output Voltage; Power is 12kW; and Switch Freq. is 65kHz.