This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28730-Q1: Problem with Datasheet calculation and Excel sheet result.

Part Number: UCC28730-Q1


Tool/software:

We are designing our Flyback circuit with 400Vin and 18Vout, 13W using this controller. 

I have used datasheet to calculate Rcs,

for an efficiency of 85% and ηxfmr of 91%, Nps = 6; Rcs can be calculated from datasheet formula as (VCCR*Nps*sqrt(ηxfmr))/(2*Iocc) = 1.104ohms

But the SLUC579 excel sheet says the Rcs is 0.617Ohms.

May I know the reason for this.

I am  getting bigger primary inductance from data sheet calculations than Excel sheet. Can we get the formulae used for Excel sheet, may be an unlocked one.

Thanks.