Tool/software:
Hi,
In the calculator spreadsheet, a junction temperature is calculated (estimated) of 64 degrees.
Under what circumstance is that, in the spreadsheet the demo board is shown? I have the demo board and with the shown input voltage (30V) and output voltage (12V) and current (3A), the junction temperature is much higher at 81 degrees measured with a FLIR.