This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG2100R044: HS min on-time

Expert 4750 points
Part Number: LMG2100R044


Tool/software:

Dear E2E Support,

Can we share what is the High-Side ton(min), or how to calculate it, to stay in a safe operating area vs the bootstrap capacitor charge?

Regards,

  • Hi ,

    There is no straightforward answer for the high-side minimum on-time as it is very application-dependent. 

    The main item that should be insured is keeping the HS-HB voltage above the device's UVLO turn-off threshold (3.7V maximum) to prevent it from shutting down. 

    To ensure that this voltage remains at an acceptable level, the simple capacitor voltage-current relationship can be used: i = C * dv/dt.
    In this equation,
    -i is current consumption of the high-side device.3.5mA can be used here.
    -dv is the voltage droop in the capacitor when the high-side is on.
    -dt is the time that the high-side is on.
    -C is the bootstrap capacitor value. 

    C should be designed such that the voltage droop (dv) does not fall below the maximum UVLO turn-off threshold and with some additional margin.

    As an example, let's take the case of a buck converter operating at 500kHz with an 80% duty cycle on the high side. Here the period is 1/500kHz =2us and the high-side on-time is 80%*2us = 1.6us. Assuming the VCC voltage is 5V, the bootstrap capacitor will get charged to Vboot = VCC - Vdiode = 5V - 0.9V = 4.1V

    Then, when the high-side is on for 1.6us, the capacitor voltage droops according to Vdroop = dv = i/C*dt. 


    Now, we design for the value of the bootstrap capacitor - if I want to keep Vboot above 3.7V, say about 3.9V, Vdroop must be equal to 0.2V.

    Therefore I can rearrange the equation above to solve for C: C = i*dt/dv= 3.5mA*1.6us/0.2V=28nF.

    Thanks,

    John