Other Parts Discussed in Thread: BQ25895, , BQ25890, TPS2121
Tool/software:
Hi,
I am using the TPS61022 for 5V 3A boost from the SYS output of my BQ25895. I wanted to get a schematic check of the whole circuit and would love feedback on how to optimize on space and component size. I have two main questions, 1) since both my inductors are close how bad will the EMI be?
2) Previously, when no battery is connected and I was using the PMID 5V 3.1A built into the BQ25895, I would sometimes get a low voltage error on my CM5 when under heavy load, this disappears when a battery is attached. How can this be rectified? More capacitance? Would love some insights!
Schematic:
I have not made the ground pour visible for easier readability but there will be bottom and top ground pours. This is a 6 layer PCB with 2 additional internal ground planes and a +5V plane.