Tool/software:
I see in the Datasheet, Forum, and Schematic Checklist when the BQ25895 is used with OTG, that a capacitance value of 40uF is needed to achieve 2.4A output, while a value of 60uF is needed to achieve 3.1A output. There is no calculation provided in the datasheet that I see clearly to determine the value of capacitance for this usage. I am considering a 58uF, 68uF, or 100uF capacitor to work in place of a 60uF as it seems much harder to come by. I am curious on how it will affect the circuit if I go over 60uF ?6330.BQ25895_5F00_SchematicChecklist-V1p0.pdf