Other Parts Discussed in Thread: BQ25750
Tool/software:
Dear TI Support,
I am designing a USB Power Delivery (PD) application as a 100 W sink, powered from a USB Type-C PD adapter (controlled by the TPS25751D) and charging a 7-series supercapacitor bank (2.7 V each) using the BQ25756.
In my design:
-
The TPS25751D negotiates 20 V/5 A from the PD source.
-
The BQ25756 is used to charge the 7S supercap bank.
-
The system load (board) should normally be powered from the USB-C PD adapter, but must also operate from the supercaps for a few seconds if the input power is suddenly removed.
I selected TPS25751D + BQ25756 because this pairing is fully supported together in the USB PD Application Customization Tool (GUI Composer).
However, I have two concerns and questions:
-
Power-Path Management
Since the BQ25756 does not have integrated direct power path, what is the recommended approach for switching the system load between adapter power and the supercap bank?-
Do you have a reference design showing this kind of power-path control with BQ25756?
-
If not, can you recommend a switching circuit (e.g., ideal diode controllers, power multiplexers, or FET-based load sharing) that TI recommends for this use case?
-
-
Supercapacitor Balancing
For the 7-series supercap bank, do you recommend using a balancing IC to maintain voltage distribution across the caps?-
If so, can you suggest a TI balancing IC that would best complement the BQ25756 charger in this design?
-
Ideally, such an IC could also simplify integration with the charger.
-
I would greatly appreciate your guidance or reference material for implementing TPS25751D + BQ25756 in this configuration.
Thank you in advance for your support.
Best regards,
Mohammad Kireany