LV5144: Question about LV5144 EVM.

Part Number: LV5144
Other Parts Discussed in Thread: LM5146

Tool/software:

Hello guys,

One of my customers wants to evaluate LV5144 using EVM.

But LV5144 EVM is not available.
At this moment, they have the following questions.

Could you please give me your reply?

Q.
LM5146 EVM(LM5146-Q1-EVM12V) is available.
But since the LV5144/LM5146 have power pad and soldered to board,
I think it would be difficult to replace the LM5146 with the LV5144.
Also I think LV5144 characteristics are almost same with LM5146 one except the maximum input voltage.

If I check the characteristics using the LM5146EVM without changing to LV5144,
are there any items that will cause a significant difference from the characteristics of the LV5144?

Do we have to replace the LM5146 on this EVM with LV5144 to evaluate LV5144?

Your reply would be much appreciated.

Best regards,
Kazuya.