Tool/software:
I would like to know if it is possible to operate the TPS26750EVM at a 240W output without using GPIO6. Additionally, I’m looking for board data or documentation that shows the location of R24 on the TPS26750EVM. Lastly, I’d like to understand the function of SBU1 and SBU2, and whether the board can operate normally without them.