Other Parts Discussed in Thread: LM51772,
Hi,
This is an urgent request for assistance in designing a 5V power supply using the LM25141.
- Vin range is from 6V - 36V
- Vout 5V @ 12A
This is our second attempt to design this power supply. Our first attempt used an LM51772 buck boost with a Vin of 4V -30V range. This failed miserably! Please reference the TI forum link here.
Our customer has requested that we redesign this power supply using the new Vin stated above. We decided to use the LM25141 Buck controller since we have already implemented a working 3.3V 16A version on this design and want to simplify the design process. We have an extream short respin time because of time lost with the first attempt.
Using your Webench online tool, we are getting slightly different values and components compared to the 3.3V version. So would need assistance in comfirming this new 5V design and verify that the working 3.3V version will also work with this new Vin requirement. We'd would prefer not to have to redesign the 3.3V at this time.
Would you please assist us?
Thank you,
Mark Vandewaetere