Hi!
We are going to use TPS40400 to get adaptive voltage scaling for TMS320C6A8168, but we need to get right power sequence for proper processor operation.
TPS40400 will make 1V AVS and this voltage should start after 3.3V has started. To get right voltage's sequence here must be EN input in TPS40400, but here is only CNTL pin which can behave dependent on programmable parameters in TPS40400.
Question: what is the default behaviour for CNTL pin?
We need that it behaviour would be like EN pin without any commands by PMBus. We don't have any adapters to programm TPS40400 before assembly it on PCB.
Thank you.
Sergej.