This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65994AE: TPS65994AE I2C Port functionality and mapping

Part Number: TPS65994AE

The TPS65994AE datasheet lists the following for the i2c ports:

  • I2C_EC, slave, connect to embedded controller (EC)
  • I2C2s, second slave port

We have a host processor (SOC running Linux) and an ASM4242 USB4 controller in this system. The reference designs show the ASM connected to I2C_EC. Is this correct?

Functionally, what is the difference between the I2C_EC and I2C2s ports? Can they both accept the same commands and do the same operations, or are there limitations on one of the ports?