We are looking to use the TPS51916 in a 3.3V-1.5V (plus VTT) DDR3 application. It will be supporting 2 banks of 72 bit DDR3 (9 devices).
First: It appears the V5VIN current is always <1mA regardless of load or temp. Since we do not have a 5V rail available (and want to minimize cost/size), can this be supplied from a reference voltage (say 12V->5V reference or zener)?
Second: Is the 2A limit on the LDO VTT supply enough to support 2 banks?
Thanks!