This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51315?

Guru 13485 points
Other Parts Discussed in Thread: TPS51315

need a DC-DC converter that can produce out of a low voltage input an output for the core of my CPU : from 5V input to 1.05V @ 6Amp @ 85cambient !!

I searched in the Switcher Pro and found that the TPS51315 can do this task.

1. Do you have a better suggestion (make sure that also after the 85c derating still it can provide 6 Amp) ?

2. Do you agree that the TPS51315 can provide the above 6Amp also at 85c ambient ?