Dear Team,
We have got a customer which is AMStech.
The customer is targeting for Smart Grid.
So the customer worried about the over charging current.
When the model is charging the battery( 3.3V), the over current is up to 700mA~ 1A.
Our datasheet is guarantied by 500mA.
But when the Short-circuit trip current is by 1.6A
So is BQ24202 available to use the custome specification?
Please refer below the specification.
1. input voltage: 5V
2. output voltage: 3.3V
3. charging output current : 700mA ~ 1A
When I reviewed the circuit, it seems to be all right.
Also I attached the schematic file.
If you have got good solution and idea, Please reply to me.
Thank you.