Hello! It's me again. I was just wondering what's going on with my 2KW PFC circuit using ucc28019. I was finally able to make it work, I put a small load on it, it outputs a more or less steady 385Vdc, at 0.8A. The problem I'm seeing is the inductor current, whose waveform is attached here. I was wondering where the spikes near the peak are coming from? From the zero crossing it's quite steadily rising, and then as it nears the top it goes crazy. My superior says it has something to do with over compensation? Or the fact that I'm not using the rated load of (supposedly) 2KW. Please advise. Thank you very much! (I'm attaching the latest schematic after this post)