Hi,
I'm working on a project including the OMAP4460 and TWL6030. Very similar to "Pandaboard". Now I experience the following:
I supply power (3,7V) to VBATT, I see all voltages ramping up on my scope. Just when the last voltage is fully ramped up, I see the power off sequence. NRESPWRON is never set by TWL. VIO1,8 is up for just 15,5ms. I see all voltages going down like shown in the datasheet. All voltages seem to reach full level, so I guess there is no short circuit.
Maybe I'm getting something wrong, but should the power on state last at least until the watchdog timer disables the device? Even if the OMAP is not responding? Since NRESPWRON is never released to HI level the OMAP will not start to boot.
Would a "short circuit" on a single rail result in a shut down? Or will it disable just a single rail.
I see VRTC present all the time. Also the 32khz clock is running. When I manually set the "PWRON" the whole sequence happens again. Power ramps up, power shuts down.
Thanks for any help on this!
Ole.