Hello,
I have designed a SEPIC with LM3478, with the following specs :
Vin : 8V .. 19V
Vout : 12V
Imax : 6A
The design is a mix between Webench (see webench_design_744428_44.pdf) 4760.webench_design_744428_44.pdf and my own calculus from AN1484 and LM3478 datasheet. The final schematics is here attached (ugbCV12V.pdf).4062.ugbCV12V.pdf
L201 is Vishay IHLP6767GZER220M01 (26.5mOhm max DCR)
L202 is Vishay IHLP5050FDER100M01 (17.2mOhm max DCR)
The SEPIC behaves as :
- with no load, Vout is 12V on 8V .. 19V Vin range ; audible noise is heard (MLCC or self ?) : OK
- with 20 Ohm load (0.6A), Vout is 12V on 8V .. 19V Vin range : OK
- With 10 Ohm load (1.2A), Vout is 12V from 19V down to around 10~11V ; under this limit, the T203 gate is not driven correctly any more, a sharp noise is produced, and Vout is not kept at 12V any more. L201 gets rather HOT ... NOK
Hence I wonder what is the reason for that behaviour, and more over if this design will be able to provide 6 amps on the expected input voltage range. Can you, power experts, provide a clue ?
Many thanks
Laurent