Hi,
Can somebody provide the design details of a UCC28700 based power supply with the following specs :- Input voltage range from 100V to 300VAC and
Output of 12V at 800mA
Kindly verify the design that I have tried to do
8883.UCC28700_excel_calculator 12V 0 6A.xls
Is there any test procedure for checking a power supply built with UCC28700 ?
I am awaiting a reply
Regards
Atul Bhakay