This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3906 question

Other Parts Discussed in Thread: UC3906

I've been assigned the task of designing the charging circuit for my senior design project. I've chosen the UC3906 to charge the two 12 V SLA batteries that I've put in series. I've read over the spec sheet and U-104 application notes numerous times and set up my circuit using Figure 13 of the U-104 application notes as a reference. I used the design equations from the spec sheets to obtain the resistor values needed to set up the dual level float charger. I set my over-charge voltage at 29.1 V, the floating voltage at 27.3 V and my turn on voltage at 20.4 V. Below is the schematic for my design. 

I am not getting the correct maximum current into the battery during operation. Using the .470 Ω resistor, the maximum charging current should be around 530 mA. I am getting double that, around 1.1 A,  into the battery during charging.  Could it possibly have something to do with ∆V across the TIP32B? Any help with this problem would be greatly appreciated.

  • Please measure 0.47 ohm current sensing resistor voltage drop. It should be 250mV+/-25mV.

    If voltage drop is in range, then check resistor value.

    If voltage drop is not in range, probably IC is damaged (at least out of spec).

    Input should have enough decoupling capacitor.

    IC is rated as 40V, 36V power supply hot plud in may have high voltage overshoot spike, may damage IC.