Hi,
Please help with the following questions,
1- I understand that if the unit is powered with the DC Voltage Vac the D5 goes on and D4 is on when the battery is charged through USB. What are the D2 and D3 indicating?
2- How long does it take a battery to be charged?
3- I understand that USB high power it can be set in the control panel. Does this mean that some computer can not provide the 500 mA through the USB?
4- When do we know that the battery has been charged completely?
5- Is ther certain battery that can not be used by this I.C?
Thanks,
Ali.