This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118 design spreadsheet question

Other Parts Discussed in Thread: LM5118, LM5117

Hi,

I am using the LM5118 Quick Start Component Calculator to design for 16V - 32V input, 30V @ 5A output. The output will ramp between 1.23V and 30V and I wanted to see what the calculated values were down to 1.23V output. However with output below 11V, it is no longer in buck-boost mode operation and the calculator doesn't give values for peak inductor current, current sense resistor, and error amplifier compensation. I understand the LM5118 will start operating in buck mode but why does the calculator not calculate those values in this range?

0654.LM5118_Calculator 1040 heater 150W.xls

Thanks in advance for the help.

 

Regards,

 

Brian Wang