I would like to know the specification on ht e flyback transformer used in the "High voltage isolated DC/DC converter with 30 to 800V input and 24V @ 250mA output" reference design PMP7763 . It is named T100 in the schematic "GCI Technologies" part number: G094173LF. I was not able to find this part on GCI Technologies website. So i would like it if someone can tell me what the transformers Electrical Requirements are.