This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM-5010 RTN PIN



Hello!

I have a project for the input range 60 V max. DC & output 8.4V , for this purpose I selected LM-5010A IC. I prepared schematic using webench designer. In this the system do not grounded the RTN pin , although I checked in datasheet it is been grounded for internal circuitry. Kindly tell me whether it is intentionally not grounded or it is system error. I attached also the design.6371.8.4V Circuit.pdf

Regards, Mohit Chopra2548.8.4V Circuit.pdf