Hi!
I am part of a solar racing team that has designed a Maximum Power Point Tracker (MPPT) using the SM72442 controller and SM72295 bridge driver. We based our design off of the SM3320-BAT-EV reference design.
Changes from the reference design:
- Changed input and output voltage dividers
- Create voltage rails off of external 12V rather than solar panel
- Modified power electronics for our specs (different voltages/currents)
- (accidental) Moved VOUT voltage sense to the output side of the current sense resistor (note: I tried flywiring it back to the other terminal of the sense resistor with, predictably, no change)
- Completely new microcontroller/non-Solar-Magic chips (these work)